Am interfacing DIRIS A40 energy meters via profibus to AC450, where do get PBSD User_Prm & Cfg data to insert
In PBSD database there are information from GSD file that are to be inserted in: User_Prm_Data 1 and Cfg_Data
From gsd file how do one identify such information. This is the most difficult area to configure, where can one find detailed manual how to configure PBSD database?
From gsd file how do one identify such information. This is the most difficult area to configure, where can one find detailed manual how to configure PBSD database?
Answers
You can have a look at my app. Or you can use the profibus tool delivered with Control builder A, with simple gsd files it works. If you have IO system you might have to strip the gsd files to parts you use and then proces it (remove the modules you don't use from the gsd file)
Add new comment