error 1603 installing 800xA SV6.0.3.2 on server 2012 R2
Hello,
I'm getting this error when running system setup.
I've tried running 6.0.3 and this works fine. but 6.0.3.2 is not OK .
anyone ?
![]()
/12/2018 3:26:05.645 PM -> Information: Copy media completed.
7/12/2018 3:26:06.655 PM -> Information: Node preparation state was saved.
7/12/2018 3:26:06.811 PM -> Information: Starting prepare actions...
7/12/2018 3:26:06.980 PM -> Information: Invoke command 'Uninstall SI' Path: msiexec.exe.
7/12/2018 3:26:09.361 PM -> Information: Invoke command 'Installing the system installer agent with MSI.' Path: msiexec.exe.
7/12/2018 3:26:20.334 PM -> Error: Command 'Installing the system installer agent with MSI.': exited with error code 1603.
I'm getting this error when running system setup.
I've tried running 6.0.3 and this works fine. but 6.0.3.2 is not OK .
anyone ?
/12/2018 3:26:05.645 PM -> Information: Copy media completed.
7/12/2018 3:26:06.655 PM -> Information: Node preparation state was saved.
7/12/2018 3:26:06.811 PM -> Information: Starting prepare actions...
7/12/2018 3:26:06.980 PM -> Information: Invoke command 'Uninstall SI' Path: msiexec.exe.
7/12/2018 3:26:09.361 PM -> Information: Invoke command 'Installing the system installer agent with MSI.' Path: msiexec.exe.
7/12/2018 3:26:20.334 PM -> Error: Command 'Installing the system installer agent with MSI.': exited with error code 1603.
Answers
The 1603 error is a standard error from the windows installer system (from .msi) file. It looks like if the uninstall SI (system installer agent) didn't work correctly and that therefore the installation of the new version fails.
Try installing security patches and then try reinstalling
the problem was an "-" in my netbiosname
Add new comment