Advacommand 1.8/2 for Unix for Master
Good Morning , Could you support to us in the following issue ?
Customer has installed 4 workstation as Operator Station version 1.8/2 because they have had some problem regarding to UPS and external feed power , 3 of them has gotten problems because they had gone to shutdown suddenly ( improper way ) , they have tried to run fsck but is has not repaired the files and the outcome has been , file system corrupt volumen 4 , root filesystem corrupt , please run fsck but we have run it , then message COULD NOT FIX FILE
Customer has installed 4 workstation as Operator Station version 1.8/2 because they have had some problem regarding to UPS and external feed power , 3 of them has gotten problems because they had gone to shutdown suddenly ( improper way ) , they have tried to run fsck but is has not repaired the files and the outcome has been , file system corrupt volumen 4 , root filesystem corrupt , please run fsck but we have run it , then message COULD NOT FIX FILE
Answers
If answering ”y” (yes) to fsck does not give positive result a total reload is your best & fastest way out.
Boot on CD or DAT-tape (with install media inserted) answer some questions (name, IP, SW-options, etc) and 30-60 minutes later the machine should be ready for a restore of process graphics (Restore of OS Configurable Data) or Display Transfer (over Ethernet).
Boot on CD or DAT-tape (with install media inserted) answer some questions (name, IP, SW-options, etc) and 30-60 minutes later the machine should be ready for a restore of process graphics (Restore of OS Configurable Data) or Display Transfer (over Ethernet).
by ricardo.marrero.a Rank: 157 on 7/4/2018 5:00:40 PM | Like (0) | Report
Hi Stephan , Thanks for your response , please do you know the catalog number of the book to install the OS ? Installation manual or the user guide
Thanks for your support
Ricardo
Add new comment