Alarm Property Server
Hi,<br>We have front end SV 5.1 FP4 RevE<br>I want to know after this version , In which RollUp ALARM PROPERTY SERVICE is incorporated. <br><br>what is significance of ALARM PROPERTY SERVICE ?<br>Appreciate if anybody can give me link of details/release notes of Rollup in which alarm property service is incorporated in xa.<br><br>Thanks in advance
Answers
The Alarm Property Service is incorporated form Roullup "800xA Base S-FP 5.1.4-2 RU1" onwards refer Doc. Id. 3BSE085474
The performance has been improved by introducing a Alarm Property service that provides and caches the alarm status data for all tabbed workplaces in the system. This reduces the load on the aspect directory and improves startup and navigation performance for all tabbed workplaces which uses alarm properties that uses the PG2 graphics as alarm filter.
It is necessary to configure the Alarm Property Service after installation of the Rollup.
The performance has been improved by introducing a Alarm Property service that provides and caches the alarm status data for all tabbed workplaces in the system. This reduces the load on the aspect directory and improves startup and navigation performance for all tabbed workplaces which uses alarm properties that uses the PG2 graphics as alarm filter.
It is necessary to configure the Alarm Property Service after installation of the Rollup.
Add new comment