AC500-ECO CPU
Hey
I have a project which Content 654 Digital Input , 223 Digital Output , 155 Analog Input , 35 Analog Output .
So My Question is what is the maximum Digital Input . Digital Output , Analog Input , Analog output For Ac500-ECO That i can use .
Thank you .
I have a project which Content 654 Digital Input , 223 Digital Output , 155 Analog Input , 35 Analog Output .
So My Question is what is the maximum Digital Input . Digital Output , Analog Input , Analog output For Ac500-ECO That i can use .
Thank you .
Answers
Hi,
Please find below the IO count details from AB help file.

Since the number of IOs is larger than that what can be connected on the IO bus beside the Eco CPU, you will have to use DC551-CS31 Modules to add additional decentralized IOs on the CS31 bus (COM-1 only and max 7 modules beside each DC551).
Below are the limitations for each DC551 module w.r.t to the maximum no of IO channels that can be assigned to different types of signals (DI/DO/AI/AO).


Regards
Rahil
Please find below the IO count details from AB help file.
Since the number of IOs is larger than that what can be connected on the IO bus beside the Eco CPU, you will have to use DC551-CS31 Modules to add additional decentralized IOs on the CS31 bus (COM-1 only and max 7 modules beside each DC551).
Below are the limitations for each DC551 module w.r.t to the maximum no of IO channels that can be assigned to different types of signals (DI/DO/AI/AO).
Regards
Rahil
Add new comment