800xA SV5.1 QuickList Operator Aspect inserted in Application Bar
Hello, I want to insert an button in the application bar to open the "Config View" of an Quick List Operator aspect.
To insert the main view is no problem. But I want give the operator the possibility to define the seach criteria for itself without the using of any browser.
Do anybody know the rules to insert the Config View of an aspect?
Answers
Create a faceplate with two tabs. One for config view and one for main view..
Hi,
You can create a small graphic display containing aspect view button (with Quick List:Config View reference) and add it to Application Bar's Fixed Displays.
But I suppose you want to add a button (an icon) to the Application Bar Shortcuts or Display Shortcuts. I solved this problem by creating a regular graphic display containing two Aspect View Wrappers side by side - one with ViewReference Quick List:Config View and the other with Quick List:Main View. Link to this display is placed in the Display Shortcuts.
This solution may be slow because searching according the last search criteria is performed during display call up, so it might be better to have only one Aspect View Wrapper (Quick List:Config View) and an Aspect View Button to display search results (Quick List:Main View).
You can create a small graphic display containing aspect view button (with Quick List:Config View reference) and add it to Application Bar's Fixed Displays.
But I suppose you want to add a button (an icon) to the Application Bar Shortcuts or Display Shortcuts. I solved this problem by creating a regular graphic display containing two Aspect View Wrappers side by side - one with ViewReference Quick List:Config View and the other with Quick List:Main View. Link to this display is placed in the Display Shortcuts.
This solution may be slow because searching according the last search criteria is performed during display call up, so it might be better to have only one Aspect View Wrapper (Quick List:Config View) and an Aspect View Button to display search results (Quick List:Main View).
Add new comment