Hi Stefan, How to activate the O2 Output for system Alarm in SM812. with redundant PM867 Module.
We have selected system alarm check boxes from the controller setting for all system diagnostics, Execution & IOs. Even using the Error Handler did not solve our requirement. After doing the setting and download the both PM867 got crash as fault.
The O2 Signal is Steady or pulse?
The O2 Signal is Steady or pulse?
by Stefan Stromqvist
AC 800M hardware, especially Safety is not my area of expertise, sorry.
Add new comment