Hight speed counter
Dear Sir,
I have to count the on/off speed of 8 pulses / second.
My query is
Can I do the same by only changing the scan time to 100 ms with DI524 module? If yes, then what will the limitation for this module? Or If will have to do it only with FC channels for my applications, those are limited in one modules.
Thanks in advance.
I have to count the on/off speed of 8 pulses / second.
My query is
Can I do the same by only changing the scan time to 100 ms with DI524 module? If yes, then what will the limitation for this module? Or If will have to do it only with FC channels for my applications, those are limited in one modules.
Thanks in advance.
by Stefan Stromqvist
Sorry, neither AC500 nor IO is not area of expertise. I also suggest studying the profile of the person you are about to direct a question to... there are others on AKS that have skills on S500 and AC500.
Add new comment