Profibus CI854 cycle time
AC800M with profibus CI854 and need to know what intervall time it is excecuted.
Baudrate 1.5M nad these other I'm not sure what those meaning
br. JArkko
Answers
Hi,
You can explore detailed description of these parameters with help of this manual:
System 800xA Control 6.0 AC 800M PROFIBUS DP Configuration (3BDS009030-600)
page 44 onwards
Hope that helps
In addition to the above answer, the most of the values in the CI854 settings are automatically calculated and adjusted by the Processor during download, for a good communication.
Usually you don't need to adjust this values. Press F1 and check also help about CI854.
Hi.. and sorry but I had allready take look on manual but still don't find what parameters tells what is cycle time of profibus communication what I was asking.
Add new comment