Using 'sdappl' function
I tried downloading the user program to SD card using sdappl. After downloading i inserted the sd card in my laptop and tried opening the project using codesys software. I recieved the following error. Screenshot has been attached.
Kindly help solving the issue.
Voted best answer
You cannot read the program from the SD card when sdappl is used!
The downloaded material is in machincode and not readable in Codesys.
If you use Control builder+ v2.2 and up you can do a Sourcecode download where the whole project is downloaded to the sd card. If you do that I would recommend a password on your project so other can not steal it.
by admin Rank: 37 on 12/29/2013 7:15:59 PM | Like (0) | Report
screenshot missing
-Admin
Add new comment