Aqua MAster 3 FLow Mter Interface with RTU
SIte has the Following Flow Meter Model : FER221300K1S4S2B1A1A2A6G7Y1 Option AS.V0.CWA/SPX
Now I Need to Read the Following Data to RTU (T BOX)
FLow Meter States that Provision as Pulse Output and RS232 in the Procured Model
0 to 1000 m3 is configured as 0 to 50 Hz in Flow meter
We Need Actual Flow and Totalized Flow to RTU
Option 1 :
Do i Need Puschase Frequency Converter 0 to 50 Hz to 4 - 20 mA?
Option 2:
Can i Use the RS232 from Flow Meter to RTU? . Do i Need any Accessories is Required for RS 232? amd Is it Possible to fetch the data via RS 232?
Option 3:
Do i need tp purchase the High Frequency input module in the RTU?
Regards,
Hariprashanna.KS
+974-70455994
Answers
This question has not yet been answered.
Add new comment