Does anyone have problems with Control Builder in FP4?
Hello, Everyone.
We are working on several projects (All in 5.1 64 Bits System Version). After installing the FP4, we had problems with extreme slowness in programs when required edit or add local variables. This problem did not occur with FP3. This makes it extremely difficult the work. Did anyone have this problem?
thank you very much
We are working on several projects (All in 5.1 64 Bits System Version). After installing the FP4, we had problems with extreme slowness in programs when required edit or add local variables. This problem did not occur with FP3. This makes it extremely difficult the work. Did anyone have this problem?
thank you very much
Voted best answer
No not seen this issue at all.. Can you be more specific, what happens when you say slow? which are the processes in taskmanager that consumes most CPU usage?
Answers
we have poblems with search function it does not work fine
Collect the CBM session logs and raise a support request with the Local supportline.
by victor oropesa Rank: 1408 on 5/8/2013 8:27:41 PM | Like (0) | Report
Hi. thanks for the reply.
The problem occurs in the Control Builder program editor and when there are more than 1200 local variables (Aproximate). When trying to add or edit a local variable, Control Builder is "frozen" for several seconds. This is made worse when you add more variables. If the number of variable is more that 2000, the work in Control Builder is really slow. For example, if we need to add 20 more variables, the work is very slow.
We tried in other engineering client in the same system, and we have the same problem. Also we create a new project without good results.
Also we checked in a different system with FP4, and the situation in the same.
Before the upgrade (with FP3) we did not had this problem.
Thank you very much in advance for any suggestions.
Add new comment