conecting acs 800 with ac 800m
We have acs 800 drive and ac 800m controller, also we have comm. card RPBA 01, and RDCO 03. Because we don't have profibus slave Ci854, is it possible connect directly acs 800 and ac 800m with optical cable?
or acs800-optical-TB820V2(we have)-optical-ac800m?
one more question, can we connect acs 800 drive with computer(drive window) without RUSB-02 converter, in any way?
is it possible connect with drive via conector type x39 for control panel?
thanks :)
Voted best answer
Hi
only for the second part of your question:
If you not have Drive Window, you can use also Drive Window Lite SW - actual version 2.95 - but in this case you need one serial 232/485 interface, named NPCU-01
I suggest you to contact your local ABB dealer network that can give you the necessaries support.
Hope this help you
Add new comment