How to dump PC source code with DUPCS or source code handling
Hello,
I have a DSPC 172 CPU in a ABB Master DCS system with MasterAid2220 and QMP260 software. I prepared a "new test CPU" with one PROM and two RWM memory boards and assembled them to have a CPU testbed. I tayped the command DUDBS and saved database file with extension .BA But when I typed the DUPCS to get .AA PC elements, an error occured that said there is no PC source code on the CPU. I tried to DUMP "PC program" with another way in 8th menu "Source Code Handling" environment instead of 7th menu that contains dump data base source code and dump PC source code in its submenus.
1-What is the reason of the errors with DUPCS or dump PC source code ?
2-How it is possible that database (.BA) source codefiles are available but PC (.AA) source code files are not?
Thanks alot.
My mail is mojtabasadeghi44@yahoo.com
Regards,
Mojtaba
Add new comment