800xA Property Transfer from Controller to OPC
Hi,
I want to do a proprety transfer from the controller to OPC (third-party Kepware Server v5). As you can see in the attach I am pointing to the Real Pca-Value and the path is correct but is it not working. If I am wrriting from Grafic Element PG2 then I am getting the value in the other end. The Property Transfer service is working fine because I am using it to get something in the controller from IEC. I am getting also and sporadic error that the property transfer cannot write into. Dose anyone knows where is the problem or if I can do this in another way? Thank you!
Answers
Hi,
Try routing the required property value from Control connection aspect. For that you need to chage the "Expression" in the end accordingly.
Ex: ControlModule:ControlConnection:Property
Best Regards
Talha
Add new comment