BasicHIHwLib Missing in 800Xa V6.0
HI i want to downlaod my Sil3 Logic in PM865 HI integrity safty controller 800Xa V6.0. but i am unable to add the 'BasicHiHwlib' in hardware libraray as its not showing/avaialbe in the main libraray and i can not connect it with my hardware config.
please help
Voted best answer
Can you confirm you have sellected the AC800M HI Extension as shown below?
If yes, can you confirm if you can see "BasicHIHwdLib 6.0-6" in....
.
ObjectType Structure >ObjectTypes > ControlSystem > Libraries > Hardware > BasicHIHWLib
Add new comment