Freelance DCS AC900F
Hi,
I am recently working to AC900F and this platform is completely new to me. In one system I got one backup for reference but this is .csv file. So at the time of importing it is not opening. How can I open this backup and see all the information. Need help.
Answers
The csv format is only an export file.
You have import this file with the engineering tool.
In case of import the tool generates a pro file where you can see all informations
The problem was that the import crashed over a certain object type FDT_ROOT. It belongs to a special feature released for a few customers only, which allows to set up a separate HART bus from the FE PC using a HART Multiplexer and DTM technology.
The current Freelance 2016SP1 cannot cope with such an object type.
The problem will be solved with Freelance 2016SP1RU03 which was originally targeted for July 2018.
Due to delays the release is now targeted for October 2018.
The current Freelance 2016SP1 cannot cope with such an object type.
The problem will be solved with Freelance 2016SP1RU03 which was originally targeted for July 2018.
Due to delays the release is now targeted for October 2018.
by Dieter Henkel
Which version of Freelance do you use?
by Dieter Henkel
Do you get any error message?
by BR Rank: 362 on 6/5/2018 1:01:03 AM | Like (0) | Report
I am using freelance engineering 2016 sp1 10.3.9142. And at the time of importing it is showing "Encountered an improper argument". In cbf popup.
by Dieter Henkel
Can you zip the CSV file you try to open and send it to Dieter.Henkel@de.abb.com ?
by BR Rank: 362 on 6/5/2018 11:23:09 PM | Like (0) | Report
Yes definately i will send.
Add new comment