AlarmControl button is pink in 800xA
Hello,
we installed a new 800xA system (6.0.3), but now in our faceplates the alarmControl button has a pink background. Anyone any idea what is missing and how I can fix this? See attachment for an image.
Answers
Pink = a logical color definition is missing.
I assume a custom library is in use (the system default AlarmControl should suffice on definitions part of factory default). Check your dependencies.
Goto Workplace structure->Plant explorer workplace->Process Graphics colors aspect
Check "FaceplateBg" resource is available or not, if available check the color and the default value should be RGB(153,185,193)
if cuztomized is used then you should know the "Backcolor" property of alarm control element in object type(ie by editing the element and checking the "Backcolor" used)
Add new comment