problem with inserting of library components to the function designer at the engineering workplace
Hi dear Rob, I have installed ABB Engineering Studio 6.0.0-2, some library objects can not be inserted to the function designer without any message! While this can be done in the diagram of the control builder envirement!
for example objects from ProcessObjExtLib 2.6-3 like MotorUniM:
Object Types\Control System\AC 800M/C Connect\Libraries\ProcessObjExtLib x.x-x\Control Module Types\MotorUniM
Answers
A customized library object should have a Function aspect, for Function Diagram to be able to accept it. Add this aspect manually for the required library object and then try to insert this object in the function diagram. There should not be any problem.
Hope this helps. :)
Hope this helps. :)
Add new comment