OPCDA is not going into service mode in system 800xA 6.0.3.1 windows server2016 OS with HARMONY connect
Hello Guys,
My system is 800xA 6.0.3.1 with harmony connect(os windows server 2016).
I have uploaded the partial structural backup and found that my OPCDA service is not running.my depolyment is error free.RNRP is working.
i have check OPCDA status in all the three way , OPCDA service group manually created through Control structure and directly into service struture and automatically created by the system.
Please help me to understand if what could be possible solution.
Answers
Please open the Server Explorer Web Based and check the HarmServer Status there. It should NOT say Unavailable. Check that there is a HarmServer Object in the Control Structure as well. Is this a new Install or Upgrade. If upgrade you MUST run the Harmony Standalaone Tool in the Old System and import this MDB filr into new System.
Add new comment