web server not working
i ve configured the control builder and codesys for web server but its not working in chrome and opera(shows plugin not supported), in IE in title of the tab it displays as codesys web visualisation but there is no content in the web page .
plz take a look in following plc details:
rtsinfo
rts version: 2.4.7.38
OS version: SMX smxPPC 3.5.2
uses IO driver interface
rts api version: 2.409
4 driver(s) loaded
driver 1: AC500 CPU driver, device interface version: 2.403
driver 2: AC500 I/O-BUS driver, device interface version: 2.403
driver 3: AC500 COM driver, device interface version: 2.403
driver 4: AC500 Coupler driver, device interface version: 2.403
AC500 PM592ETH(DISP) : V2.3
AC500 PM592ETH(BOOT) : V2.0.6,2011-01-19 (Build:10249,09:01:58,Rel)
AC500 PM592ETH(FW) : V2.3.3,2013-12-18 (Build:13337)
Voted best answer
that's right with the file!
First, I note that in Control Builder you not have define any IP adress of cpu ..... when you start IE, you must specify the IP address of plc to open and normally the adress is not 0.0.0........more info after phisically test in next w.e.

Answers
Greetings,
Please find attached two documents. One of them is AC500 Webserver Manual. So you can compare your settings according to manual.
Also for webserver Java Runtime has to be installed and configured on your client machine. The other document is about how to configure java settings on your client machine.
Hope these help you.
Hi
what version of Java are you using?
With Java 8 AC500 web server CPU need to update some file.
Check with the suggestions of the attached file.
Hope this help you, let us know about the results

i tried with the instructions given in the attchmnt., but its not working
Add new comment