scheduling a report
we want to schedule one report in excel format, in a way that every day, one report will be send to one directory, with file name identified clearly. and the content of this file will be some variables that now are being logged in standard logs, for example temperature, from 12:00 to 12:00 next day.
I was reading the IM reports manual and it appears possible, but manual also show many options that confuse me a little,
someone has experience with scheduling reports, please give some instructions how is the best way of configure this.
also if there is something that we should consider in this case.
Voted best answer
This is not easy to explain over such a forum. Please look at the IM books from recent versions there is an appendix at the back that tries to explain how this can be done. I have attached what we refere to as a "Mr Engineer" a basic walk through on Report configuration which might also piont you in the right direction.
Check associated App @
Source:
Answers
You can customize your report as per client requirement. Or you can use the standard report templates to generate daily r shft reports.
If you go through the schedule structure sample daily/shift report templates are available in 800xa system. you can refer the same.
Add new comment