PG2 proces graphics editor - Pipe color
Hello
Is it possible somehowe to define color of pipe as mixture of 2 colors as in attached file.
Pipe should be red, blue, red, blue, .....
Best regards,
Uros
Voted best answer
Answers
Hi,
I don't think it's possible to have alternate band colours on the pipe object via. standard pipe object properties. Only the inner and outer colour shades can be selected from the object's properties.
An alternative to this would be to superimpose for example Red coloured pipe segments(1cm length), 1cm from each other, on a DarkGray pipe of length 14cm. Beginning of pipe should have Red segment and end of pipe should have DarkGray segment (similar to what is shown in the attached image).
Select all the items comprising this custom designed pipe object and group them. Copies of the grouped 14 cm long pipe object may be used to extend the pipeline graphic without altering the dimensions of the constituent items (due to increasing the width of the grouped object).
Regards
Rahil
Add new comment