Trend display additional features
Dear Sir,
Right now I am using "Right View" of trend to display the trends and as per customer requirement, they want
1. Only specific trace if he presses any of 1h, 2h, 4h, 1d like for 1d of "Right:View" then only 1 day trend should display, not previous or later, however now there is no such filter or boundation on display.
2. can I display the trend value on any "Numeric Display" with any specific point of time?
Thanks in advance.
Right now I am using "Right View" of trend to display the trends and as per customer requirement, they want
1. Only specific trace if he presses any of 1h, 2h, 4h, 1d like for 1d of "Right:View" then only 1 day trend should display, not previous or later, however now there is no such filter or boundation on display.
2. can I display the trend value on any "Numeric Display" with any specific point of time?
Thanks in advance.
Answers
Use time scope end time which will be present at the bottpm of trend display "Right view" for specific time and date
Add new comment