Problem of channel I/O CI801 and Firmware
Hi ,
I want establish the communication between CI854 and CI801 -AI810 AND DI810
I find the equipement and I established the communication but I have some warnning and some error you find it in the attached I can't read the real status channel...
How can I upgrade the Firmware of CI854 .
Regards
Answers
In your firmware screen check the boxes behind the ci854 rows and click download firmware for selected units. But you also need to check what’s wrong with ethernet channel 1 and why the redundant controller is not working. For the io did you connect 24 volt to all the L1+ en L1- connectors on the terminations units from the io.
when I click on download Firmware I have thise msg "Firmware download canceled.Application exists in controller" the wiring is already done everything is correct but I can't read the real status and for ethernet port show No communication backupCPU
Add new comment