UMC100-FBP CONFIGURATION
PLEASE PROVIDE STEP BY STEP PROCEDURE TO CONFIGURE UMC100 FOR LOCAL,TEST MODE CONDITION .
LOGIC IS FOR DIRECT STARTER .
HOW CAN I ASSIGN DIGITAL INPUTS FOR LOCAL MODE ( LOCAL MODE ENABLE IS GIVEN FOR DI0 , START COMMAND IS THROUGH DI4) & SIMULATION MODE ( SIMULATION COMMAND IS THROUGH DI1 & START IS THROUGH KEY PAD)
Answers
Try to check documents on next link:
http://www.abb.com/product/seitp329/e3fb02b391df72a1c12576af00574ba8.aspx
In the section Technical description greyed documents below:
Logic is possible to change via Custom application editor:
Source:
error 17:
I assume version of application editor is not compatible - please check it.
Regarding dowloading SW - contact people for your location. All is shown on the link in the first post (right side).
Add new comment