MB300 bus error
The system is really small, only one combiened AS+CS and one AC450. The old 800xA was V4.1 now it is V6.0.3. With the new system I get a bus error freqently which I don't have seen in the old system. It comes and go with the same time stamp.
I add the event details as screenshot. The event comes from the controllers node number. All works fine so I would guess that there in not really an error.
Any idea what happens or how I could get rid of this annoying message?
/Erik
Answers
System error. The CI520/CI522 has a system error
Data2: 32-bit system error “H’40000000”
“Simultaneous Time Masters“
Several stations on the bus are defined as Time Sync Masters. Check the Time sync definitions.
Add new comment