AC900F controller Fatal Error 10000103
Redundant AC900F Controller PM902F processor and CI930F profibus module found by cutomer with Fatal Error 10000103. Error Red LED on Run not on.
Profibus has no led's on at all including power.
Power cycle brings contoller directly to that screen.
Took the faceplate from Demo controller to failed controller, said verion error.
Took faceplate of Demo to Failed, and restarted power, said Fatal Error.
Took profibus module from failed to Demo, no issue.
Took profibus module from Demo to Failed, no issue.
We have been running failed controller connected to profibus with IO for a week or with no issues.
Can anyone please let us know what Fatal Error 10000103 means?
Answers
Hi,
this error is a "general" error that can have different causes. Please contact your local support and provide the complete log file (from the failing controllers web page). How are the environmental conditions of the failed controller? Temperature, humidity, fields, vibrations etc? How many network interfaces are used? Are both controllers in failed state or has the secondary successfully taken over the control?
Best regards
Jürgen
E_NOT_EXISTS
10000103 Object or data does not exist
Add new comment