Function Diagram SIL Level
Dear All,
Is the Function Diagram language SIL 3 compatible and can it be downloaded to PM865 controller with SM811 connected(used as saftey controller)?
Thanks!
Is the Function Diagram language SIL 3 compatible and can it be downloaded to PM865 controller with SM811 connected(used as saftey controller)?
Thanks!
Voted best answer
Greetings,
Do you mean Function Designer? If it is, you can not build SIL certificated applications with Function Designer.
For more details please see Engineering Studio Function Designer manual.
Hope it helps you.
Add new comment