Log on not possible in clients for first time user logon on the secondary network
Log on is not possible in clients for first time user logon on the secondary client/server network on with primary client/server network switched off.
Log on is working ok on the primary client/server network on with secondary client/server network switched off.
Screen shot attached for the same.
Answers
Hello,
Which 800xA version are you using ?
How did you configure the Primary and Secondary network adapters ?
Verify your DC - does the test "Replicate Now" work ?
Did you configure Reverse Lookup Zone ?
/Ronny
Hello,
Check the following:
1. prefered & alternate DNS servers.(if you have PDC & ADC) should be configured for secondary client server network.
2.Chekc the address resolution for the secondary ip using ping -a (in system version 5.1 onwards) else check the forward & reverse lookups (for xA 4.1 to 5.0 versions).
3.network firewall should be disabled.
4.Check the network binding order.
Add new comment