OPC Server for MOD300 - Interface Problem
Dear all,
This question is related to Mod300 DCS system. I have an problem with an OPC node configured into DCN network. This OPC interface provides data to Infoplus21 server. It works well most of the time but suddenly the service omfPM.exe increase the CPU usage to 100% and the interface hangs up. Also I have observed that the use of virtual memory (pagefile) increase too.
Next, software details:
OS: Windows 2000 Server with SP3
OPC Server for MOD300 (version 1.01.035)
OMF (version 1.06.01.00)
I would really appreciate your comments and support.
Regards,
Patrick Olguin
This question is related to Mod300 DCS system. I have an problem with an OPC node configured into DCN network. This OPC interface provides data to Infoplus21 server. It works well most of the time but suddenly the service omfPM.exe increase the CPU usage to 100% and the interface hangs up. Also I have observed that the use of virtual memory (pagefile) increase too.
Next, software details:
OS: Windows 2000 Server with SP3
OPC Server for MOD300 (version 1.01.035)
OMF (version 1.06.01.00)
I would really appreciate your comments and support.
Regards,
Patrick Olguin
Answers
It appears to be a bug, which may be already fixed in another version. In order to confirm that, you shall report to ABB supportline in your region seeking support for it and may be required to upgade to latest version.
Add new comment