i have 800 xa system on paper machine dcs and qcs gettin flood with this error
hwerror pm10ac~generic(0000) status ok 9950 in system alarm list,
it is qcs and dcs system, qcs controls weight profile and mousture of paper it is smart platform it has several 800 controllers about 6 op stations for as version i do not know the alarms come in under system alarms
Answers
Please open and go online with control project in Control Builder M.
Most (all?) hardware errors and statuses will be decoded into some plain text message. Errors show up in red, warnings in yellow.
Probably, there is some hardware error or misconfiguration. It is very common to leave all IO channels enabled while using only a subset (eg on a DI810 digital input card). Not connected loops will fire "Underflow" hardware errors on every application download.
Ultimately, you should seek advice from the entity/project that delivered the control application.
/Stefan
by Sumit Gargav
Edited by Admin: merged information from previous similar thread.
Add new comment