Bailey infi90
Hi Friends,
I want to prepare IO list for exsiting Bailey infi 90 control systems. As i have backup of control system and composor software.
How can I export input /output tag list in .xls format including hardware part number.
Thanks in advance.
Voted best answer
If you want a I/O list of field termination devices it isn't that easy. There are not detailed hardware part numbers in any Composer or HMI configurations. For each termination from a field device to a DCS I/O input or output there is not a identifier or tag.
Answers
Every traditional IO card (Rack based) has a specific Function code (or two) associated with it (see attachment-I have not been able to link. Please PM me at ingo.patzer@au.abb.com to request). Using Composer and associated Power Tools, you can extract a list with these Function Codes and then us other tools to gain the list you require.
Newer IO, such as SD IO and S800 is more complicated as each channel uses a generic Function Code to define and you have to look for the specification to determine IO type and channel. This should also be done via Composer Power Tools, but I have not done this in recent times.
Regards.
Newer IO, such as SD IO and S800 is more complicated as each channel uses a generic Function Code to define and you have to look for the specification to determine IO type and channel. This should also be done via Composer Power Tools, but I have not done this in recent times.
Regards.
Add new comment