OPC FF Defination
I have one 800xa system with:
1 redundant connectivity server
1 redundant Aspect Server
1 Redundant Domain server
6 OWS
2 EWS
and my project has 100 FF device.
OPC Server FF combined into the Connectivity Server.
Each connectivity server has 2 connection with Control Network and 2 Connection with Client/Server Network.
Is it necessary Connectivity Server connect to the HSE subnet with Independent network cards?
Do I need to install a separate network card to connect to the HS Enetwork?
Answers
I believe the answer to both of the questions is no. The HS network can link the LN modules on any ethernet network.
Add new comment