Autoclose faceplate 800xA
Is it possible to autoclose a faceplate after for example pushed a button in the faceplate element?
Voted best answer
You can use this app which was recently published here on AKS:
http://www402.abbext.com/script-to-close-popup_1-0_a12818.aspx
you can try it and see if it works for you.
by sinbernal Rank: 672 on 5/8/2018 1:02:35 PM | Like (0) | Report
Hello!
Has anyone tested this scrip with sv6.0.3-1?
I still getting a error when trying to run the script: Object doesn't support this property or method: 'oShell.Sendkey" at line 5
Add new comment