Display status such as controller up /down /Io status in all,5.0 sp2
Dear all,
Could you please let me know as to how i can display controller up/down,IO status and various other system related statuses on HMI on an 800xa 5.0 SP2 system .What are the properties that i need to use to fetch these details on HMI.
Answers
Not sure which controller you are mentioning here.
If its AC800M, you can use the function block "System Diagnostics". This block is pretty handy if you want to fetch the controller status and statistics to hmi.
Hi,
If you are using 800M controller, you can retrieve HW status from "ExtendedStatus" information or you can define a variable in "UnitStatus" in connections to fetch HW status.
For further reference you can also refer control builder help.
Add new comment