How many bit of operation which Linear Flashcard works on AC450 and AC410
Hi Stefan,
I have a question about bit of Linear Flash card which is used to store System software and backup Application on AC450 and AC410 (MB510 card).
I'm buying Linear Flashcard (Pretec brand) for my controllers (installed in year 2002). At first, I request 8 bit flash card because I thinks if controller can work at 16 bit, it also works with 8 bit.
But supplier informs that Linear flascard Intel series 100 doesn't have 8 bit any longer. Just only 16 bit.
Can you advise me if 16 bit flash card can be applicable in AC450 and AC410 (Safeguard configuration)?
Thanks in advance,
Vu,
Answers
I'm not sure, I was not even aware of that multiple types existed.
My colleagues states that the flash card ABB is selling has been tested & certified for use with Advant Controller 400 (some effort has been invested in finding a suitable card).
I suggest ordering from official pricelist, or try something else at own risk.
Add new comment