Network share issue, Windows / 800xa different rights
Hi
I have a strange Issue since i made a update to V6 (Server2016/Win10LTSB2016).
First i tought it must be a access right problem, but if I logon with full admin rights, i get the same result.
If I go to the windows explorer, i can see every network drive and I have full control rights. But in the Plantexplorer, i do not have access Rights. Is there any setting for network connect in 800xA. Or a new AD-Setting in Windows?
i have used this in 5.1FP4 very often. Primary for redundant saving Reports. Like this:
\\As0011\as11_d\Reports\SETP\AC\SETP_Report_AC_<TimeStamp>.pdf
\\As0012\as12_d\Reports\SETP\AC\SETP_Report_AC_<TimeStamp>.pdf
But since the update, i always get a Error:
"unable to export to file: SETP_Reportblablabla.pdf"
Does anybody have same issues?
THX
Answers
Try inverting the LogOver setting (ON->OFF or OFF->ON) and see if it changes the behavior (with LogOver enabled, the workplace will elevate on launch)
I have LogOver enabled and I can "Attach" then type \\server\c$ to load a document off another computer's disk.
Add new comment