Is it possible to change Font Size for Obejct Name on 800xA Faceplate? if so, how?
We have requirement from customer that, object name on 800xA shall have font size more than what we have by default. Has anybody carried out such kind of changes on Faceplate framework earlier? Please suggest workaround, if any.
Thanks
Voted best answer
Some graphic libraries are protected against changes (e.g. AC800 Connect) - what graphic library are you making use of?
The best results are probably achieved if the faceplate contents is designed to meet your customer's expectations regarding font sizes, etc.
Have you contacted the supplier of the process graphics library you are using?
Even if process graphics scales (faceplate elements and contents will be stretched to the size of the faceplace frame) the result of making the faceplate frames larger is not ideal.
Another approach may be to use Windows settings to enlarge screen fonts
However, not all components of the workplace layout will scale.
Below I've inserted an example of a full screen workplace at 150% vs. 100% font scaling in Windows (reducing screen resolution is not recommended on digital screen devices - they should be configured with their native resolution to avoid blurring)
Enlarged to 150%
100% (default)
/Stefan
by Sumit Gargav
Hi, Got information from L3 support colleagues that it is not possible. But I keep question still open if someone comeup with any workaround.
Add new comment