HIGH SPEED INPUT in DC523,DC532
Dear sir,
am using DC523,DC532 with PM583 PLC.how to configure the High speed input in ABB CONTROL BUILDER ?
how to programming in codesys to measure the RPM of the motor?
(motor rpm is 8000 rpm)
Answers
Greetings,
For using High Speed Counters, you have to configure some settings according to your IO Modules. After configuration has finished you have to use CNT_IO
Function block to read RPM (or etc.) values.
Please find attached files, one of them is user manual about HSC and Configuration. The other one is eCo Series PLC HSC example application.
Hope these help you.
Add new comment