Problem alarm input panel builder 5.1
Hello,
I have a problem when entering new alarms or editing exisiting ones in Panel Builder 5.1.
When typing the alarm text, after every keyboard stroke, the cursor moves back to the initial position within the text box, making it impossible to type anything useful.
Then when clicking OK, an error message appears:
"Entry is not valid."
"May not be blank"
So it remains impossible to work with the alarm list.
I have Panel Builder 5.1/0 Build 358
Any help would be appreciated.
Thanks
Add new comment