is it possible to recover a downloaded program from a AC800 Controller?
Hi, there is a controller in a Plant, that was configured a long time ago, i was told this was on 2009, but this controller was configured with a compact control builder station, and that station doenst exist anymore, also the people from the Plant, doesnt remember the version used of the CCB, and i need to recover the program in this controller, exist any way to recover the program in a situation like this?
Voted best answer
Hi,
That issue is discused many times in AKS. Without to have an actual version of Control Builder proect (saved somewhere), it is not possible to do that. It is not possible to upload the proect from the controller to the PC with control builder.
Do you have a CF loaded in the CPU?
Add new comment