REDUDANT PM866 WITH BC810 FATAL ERROR
Fatal Errors, that reset the Processor that goes into factory default. Total load is at 96%, cycle load at 45%, memory at 70%.
It always before this error like some Hot swap of modules of communication.
the chasis has 3 redudant CI867 and fieldbus card.
Answers
This question has not yet been answered.
Add new comment