ac800f errror
Hi,
we have redundant AC800F processor and a redundant Profibus line. once,duty controller switch to redundant and after that shutdown. In log file we found this messages:
Redundancy Toggle ->Prim 0x 00000001 1. 4. 18 11: 45:22.585
Error OxFFFF0121 in REDTGL.d Line 831 1. 4. 18 11: 45:01.768
Error OxFFFFO051 in REDTGL.d Line 777 1. 4. 18 11: 45:01.765
Error 0x1001012A in PMDEVFC. Line 2447 1. 4. 18 11:45 01.461.
Error 0x100 1012 A in PMDEVFC. Line 2447 1. 4.18 11:45:01. 460
Error 0x80000310 in Times et Line 0 14.2 18 2:57:31.000
Restart due to Redundancy Boot
Error 0x80000310 in 14.2.18 2:57: 18.833 Timeset Line 0
Restart due to Initialize command 14.2.18 2:57:01.000
Error OXFFFFFFFF in REDKAL.d Line 2079 14.2. 18 2:56:33.836
Error OXFFFFFFFF in REDKAL.d Line 2079
Error OXFFFFFFFF in REDKAL.d Line 2079
Answers
Hello qanavati.sh,
You should contact L3 Support through Your local ABB contacts and send them Your full logs from both CPUs.
Hope this will help,
Mike
by JuergenV Rank: 69 on 4/11/2018 12:33:45 AM | Like (0) | Report
Freelance version?
Add new comment