Cannot create a New Project in Control Builder M
Dear All,
Please suggest some solutions for the following error.
I am using 800xa 5.1 FP4 with demo license.
When i tried to create a new project from control builder the following error appears and project get close.
[Error] Error in Interprocess communication (Access to Devicemanagementserver failed)
[Error] License for device management PROFIBUSHART has been exceeded.
Check 800xA License server.
Transaction Failed.
The Source Code operation has encountered an error.
SourceBlocak:test
ErrorMessage:Failed to commit transaction. Write project operation is aborted!
When i check the Session Log file:
Error Code: 80004005 native message: Failed to commit transaction.Write project operation is aborted!
User message: Error writing source block location :
File: d:\br\800xa_CIT\products\CIT51FP1\BL\5.1.1.-2\atlas\source\ApplicationLayer\Sou
rceCodeStorage/Sourcecodestorage/ProjectSource.cpp
Method:CSourceStorage::Internalwritproject
Line:2227
Thanks
Regards-
msmk
Answers
Hello,
first of all you should verify your license server and license client, by running License Status Viewer. No error message in that program the problem is not a license problem, otherwise you have to solve the license server/client first.
/Ronny
Add new comment