ACS800 Crane Drive firmware N652 on PROFIBUS
1. Can I use EngDriveM control module or EngDrive function block to communicate with ACS800 with CraneDrive firmware N652 on PROFIBUS (RPBA-01)? 2. "When I connect ACS800 drive with System Control Program 7.x with AC800M controller (RPBA-01) using EngDriveM control module everything is fine. When I connect ACS800 drive with ACC800 CraneDrive application program 7.43 (+N652) with the AC800M controller (RPBA-01) using EngDriveM control module got fault MAS OSC FLT. What am I wrong doing?" Could You please help me?
Answers
I'm not sure if there is anyone on this forum who understands the CraneDrive application program. I certainly dont, but anyway ...
What is the fault code "MAS OSC FLT" and which control module is it being generated by ?- This does not sound like a communication fault which would suggest that the problem is not with the EngDriveM control module perhaps?
by Govindaraj
Edited by Admin: Your earlier questions combined into same thread.
Add new comment