800xA For Melody Installation Problem
Hi,
I want to install 800xA for Melody, but i had problems. I prepared system plan for melody. Aspect and connectivity servers without problem were installed but when i tried to install configuration server i had problems. I checked everything in installation manuals but couldnt find any solution. Can someone explain me how to install it properly? I get error message as attached here.
Answers
The error says, that the credentials you provided are invalid. It looks like you are using 800xA 5.1 system installer. Check the domain name. The domain name in the installation looks like a default domain name (IIT). Are you using the same?
Also make sure, that the path from which sql is installed does not have any spaces
E.g: Path should not Z:\800xA 5.1 Setup\800xA\DVD 1 - System Software\3rd_Party_SW\Microsoft_SQL_Server\SP3
This has spaces in the folder name, try running without spaces and proper credentials, it should work fine.
Add new comment