soft point object not showing
In Control Structure compact Hmi 5.1 i am not able to see softpoint object when going for add object.
i want to create some of the temperory varibles!
Answers
This kind of preoblem Generally occurs when the system extension are not loaded.I suggest you to have a second check if the respective extensions are loaded or not?
Hi, i don't remember if hmi 5.1 has softpoint by default, but to create instance of soft point in control structure You have to create its 'definition' - object type in object type structure...
if it is something else, You've got to be more specyfic.
Regards,
Add new comment