Errors in displays with PG2
The attached files show errors when i try to view or open some displays in Connectivity Server. This graphics can be opened or viewed without problems in Aspect Server. Also attach system report file.
For test, the system is running in virtual machines (vmware).
For test, the system is running in virtual machines (vmware).
Voted best answer
This is a typical behavior when few software is missing in the node where you get the errors. Can you use DCT to collect the software installed in all nodes and see which software is missing in Connectivity Servers when compared to Aspect Server.
Add new comment