Get back up of RTA box PU410
Dear,
In old Advant Operator station AS500, with RTA board (PU515, PU516) I can go Online by OnlineBuilder then use #DUAP, #DUDBS (Dump Database Source) command to get Full Backup of RTA board's database. And go to an application folder in that OS to copy all to store.
How do I make a backup like that on RTA of Connectivity Server (PU410)?
Answers
This can be done from the plan explorer workplace. 1. Expand the Control Structure in the Plant Explorer, and select the RTA Board object. 2. Select the RTA Board Control aspect in the aspect list. 3. Select the RTA Board Configuration tab and click the RTA Board Config button. Which opens the online builder of the RTA board node, and backups can be taken. Backup files will be saved in the below path in the 800xA verion 5.0 and before, for the new version need to check.
Program Files>ABBIndustrial IT >Operate IT>AC400 Connect>Advant Base>
Data>RTA>nodes>rta>SRCE.
Add new comment